Russia

Добро пожаловать на сайт Schneider Electric

Добро пожаловать на наш сайт.

Вы можете выбрать другую страну для просмотра доступных продуктов или перейти на наш глобальный сайт для получения информации о компании.

Выбрать другую страну или регион

  • Loading a steel slab

    Iron and steel plant

    Saving 36% of total energy consumption, the maximum value is 1.58 M € per year

    RUFR
  • Customer objectives


    • Determine the possibilities of saving energy

    • Reduce energy consumption by key production processes

    • Implement projects by energy service model

  • Project objectives


    • Identify opportunities to save energy reduce energy consumption by production processes

    • Apply a financing plan for the "Off-balance sheet model" ESCO

    • Performance – is a contract (at the expense of the return of funds from savings), payback period 3-5 years

Iron and steel works

About the client

• In a top three of largest metallurgical companies in Russia

• Yearly output of more than 10 million tons

• Increasing volume of supplies for export

Our solution

• Energy performance is a contract (at the expense of return of funds from the savings achieved) to optimize the operation of the exhauster with the technological mode of conducting melts

Payback period – 3,5 years

Wind Turbine sin sunset, china.

START SAVING THE PLANET RIGHT NOW!

Nos conseillers sont disponibles pour répondre à vos questions de 8h00 à 18h00 du lundi au vendredi toute l'année.