Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Распределение электроэнергии

            Новости: Распределение электроэнергии

            Sepam serie 10 protection relay

            • A cost-effective solution, it protects your network using just those features you actually need.
            • This is a product that is easy to set up and use, with no need for computer assistance.
            • It is compact, user-friendly.

            Protection relays constantly monitor the power network and trip the circuit breakers to isolate the faulty portion under fault conditions: overloads, short circuits, insulation faults, etc.
            Sepam series 10 provide the protection of secondary power distribution networks (MV/MV and MV/LV substations)
            Protection of buildings with MV power supply: office buildings, shopping centres, industry, warehouses, etc.
            With Sepam series 10, Schneider Electric, the world leader in Power & Control applications brings you quality at the right price.

            Make the most of your energy with the best quality at the right price.