Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Распределение электроэнергии

            Новости: Распределение электроэнергии

            Powerlogic: Class A all the way

             

            Schneider Electric was the first company in the world to receive certification for the IEC 61000-4-30 Class A power quality standard by Power Standards Lab for our high-end power and energy meters.
            This is not just a European standard - it's the leading PQ Measurement standard in the world and as more organizations and energy providers adopt the 4-30 class A standards, the PowerLogic ION8800 and the PowerLogic ION7650 meters, as well as ION Enterprise 5.6 reports, will now have a competitive advantage over noncompliant products.

            PQ data collected by these meters is reliable, repeatable and comparable to results gained from any Class A compliant device, regardless of manufacturer or environmental conditions. This also increases the validity and value of any further analysis performed with the data.

            Class A measurements should be required wherever precise measurements are necessary: for contractual applications, for verifying compliance with standards, and for resolving disputes.

            Power Standards Lab was heavily involved in the development of the IEC 61000-4-30 standard. They continue to provide guidance as the standard evolves.