Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Распределение электроэнергии

            Новости: Распределение электроэнергии

            PowerLogic PM750 and PowerView decorated

            These products as voted by the magazine's readers, increase on-the-job productivity, maximize efficiency and represent simplicity of design. The annual competition is considered the most prestigious in the industry.

            Bested nearly 150 finalists PowerLogic PM750, winning the 2007 bronze medal in the Electrical Power category and the silver medal for PowerLogic PowerView in the Productivity Software category

            For applications requiring alarms, communications and digital I/Os, the PowerLogic PM750 power meter is the most compact and cost effective offer on the market. Perfect for customers with space or cost restrictions, the PowerLogic PM750 is also compatible with the new entry-level, power monitoring software, PowerLogic PowerView. Plant Engineer readers voted it a valuable addition to the marketplace.

            The software fills a key position in the Schneider solutions offer, targeting the entry-level energy management market and bridging the gap between component-level sales and the total solutions offer. Contributing to PowerView's success is its ability to be translated easily into any language and localized according to market needs, thus speeding up the time countries can start selling the software.

            The Product of the Year awards will be presented March 31 and April 1, 2008, at the Plant Engineering Magazine Manufacturing Summit in Chicago, Illinois.