Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Распределение электроэнергии

            Новости: Распределение электроэнергии

            PowerLogic PM800 power meter receives Ethernet connectivity

            The Transparent Ready port provides fast access to energy consumption and power quality data using a standard web browser, email or PowerLogic software.

            The meter offers more integrated measurement, I/O and connectivity features than any other in its price class. It is suited to all market segments for combined power quality compliance metering, disturbance monitoring, cost allocation and demand management applications.