Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Распределение электроэнергии

            Новости: Распределение электроэнергии

            A new communication interface for Sepam:ECI850

            Sepam series 20, Sepam series 40 and Sepam series 80 could already be connected to Modbus RS 485 2, 4-wire and optical fibre, E-LAN and S-LAN networks.

            Now, thanks to the new Sepam Server Module ECI850, Sepam series 20, Sepam series 40 and Sepam series 80 can benefit from all the functions of an Ethernet network. New Sepam Server Module ECI850 is the interface between an IEC 61850 protocol Ethernet network and a SEPAM RS 485/Modbus network. 2 PRI surge arresters included, in order to protect installation.