Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Распределение электроэнергии

            Новости: Распределение электроэнергии

            Initi@tive 2007 : a great success for the Energy Efficiency and Productive Automation solutions presented by Schneider Electric

            4,000 European customers came all the way to discover solutions, applications and innovations presented through two main themes: Energy Efficiency and Productive Automation.

            On stage, 300 Schneider Electric experts, 120 conferences, 16 demonstrations, 80 booths spread over 9,500 m², and 12 different languages represented. Everything was made to let the participants choose their own journey along the event, according to their center of interest.

            - Energy efficiency:Designed to provide real-life responses to customer needs, these solutions enable efficient energy use, optimize energy costs—with savings of 10% to 30%—and make energy even more available.

            - Automation:Schneider Electric’s solutions deliver even more flexibility thanks to a new generation of intelligent automation devices.
            The Company has devised a specific approach to help customers adapt tested and validated preferred implementations to their specific needs and applications. In all, 11 preferred implementations are available.

            For more information on Initi@tive Nice, the complete press kit is available on www.schneider-electric.com Press section.