Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      Increased range Basic inductive sensors Osiprox

      Helping machine manufacturers to find the most efficient solution!

      The inductive detection function at the best possible price

      Ease of installation

      • Contributes to machine compactness, short flush mountable product
      • Wider adjustment range,
      • increased range (x2), 2 to 15 mm.

      Economical

      • Increase the profitability of your solution
      • Sold in lots.

      Reliable and readily available

      • Contribute to the performance of your machine, faultless robustness
      • Worldwide range, present in 190 countries.

      Standard range, metal and plastic, flush and non flush mountable versions also available.