Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      Ultrasonic fork sensor for the packaging sector

      A High-Tech product for a High-Tech application!

      Detecting transparency is a very demanding application.

      » Ultrasonic thru-beam type detection is THE ideal solution. It is unaffected by the shape, colour or nature of the materials.
      » This ultrasonic fork sensor is particularly suitable for the detection of transparent labels on transparent film and torn or overlapping sheets.
      » High performance, compact and very easy to install due to its +/- numeric potentiometer with teaching.

      Osiris XUVU06: a high-tech detection solution for the packaging sector that completes our extensive range of fork sensors.