Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      Signaling solutions Harmony XVC/R/S

      With the new pre-assembled and pre-cabled Harmony XVC, XVR and XVS ranges, Schneider Electric offers you much more than signaling solutions. Worldwide leader in Operator Dialogue components, we provide you  with a guarantee: guaranteed solutions for any application; guaranteed reliability in any situation; guaranteed time saving.

      Three ranges are available:

      » Harmony XVC: monolithic Indicator banks in Ø 40, Ø 60, Ø 100 mm
      » Harmony XVS: sound solutions with electronic alarms and sirens up to 105 db
      » Harmony XVR: pre-cabled rotating mirrors from Ø 84 to  Ø 130 mm.

      All theses Harmony signaling solutions use the LED technology and are manufactured in conformity with the requirements of the RoHS European Directive.