Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      Optimum miniature XUM sensors

      Environment:
      » Longest sensing distances on the market
      » High insensitivity to light sources
      » Good resistance to severe environments.

      Installation:
      » Consumption halved (ideal economy for sustainable development)
      » Significant reduction in interference between sensors
      » Ease of alignment when installing, thanks to output status LED on front face of thru-beam receiver.

      Osiris Optimum XUM:
      The miniature high performance and economical sensor that complements the Osiris Universal Osiconcept XUM0 versatile sensors featuring multiple functions (5 modes in 1).

      Metal case version for severe environments also available.