Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      ODVA certify TeSys U

      For our customers, the ODVA certification is a warranty for a seamless integration on DeviceNet.

      The behaviour of a product approved by the ODVA is fully consistent with DeviceNet network behaviour. Then, integration and maintenance of the sytem are easier (cabling, LED behaviour, network objects).

      With open communication across CANopen, Profibus DP, Modbus, AS-Interface, Advantys STB, DeviceNet and Ethernet networks, TeSys U has openess in mind.

      Whatever the network chosen, the registers addresses remain the same.