Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      Safety switches Preventa XCS

      Featuring 2 technologies (coded magnetic, and mechanical action) and 3 ranges (coded magnetic, plastic case and metal case), our offer covers the diversity of your applications.

      More solutions for equipping machines
      The extensiveness of our 3 ranges combined with the introduction of new versions of the products (new snap action and slow break contacts, new guiding accessories…) provides improved solutions to meet all your needs.

      Easier integration in machines due to compactness of products
      Due to the new products, the safey switches are now available in 2 and 3 snap action (with positive opening operation) and slow break contact versions that are more compact: only 30 mm wide!

      Increased safety of installations
      Our offer now includes products fitted with a 3rd contact specifically for diagnostics in order to improve machine availability and also, to provide better foresight in the event of a fault. In addition, specific torx screws to prevent access to the contact and readjustment of the products have been added.