Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      Harmony XALF: the solution for your lifts!

      Control in complete safety lift movement !

      Ideally suited for lift maintenance applications and establishing their conformity, Harmony XALF control stations feature modularity and simplicity for incorporating Harmony XAL/XB5/XB7 ranges of control and signalling units.

      Three types of boxes available:
      • Top of car boxes.
      • Pit switch boxes.
      • Hoistway boxes.

      Conformity to standards: IEC/EN 60947-1, IEC/EN 60947-5-1, IEC/EN 60947-5-4, IEC/EN 60947-5-5, EN 418 (trigger action latching Emergency stops) and EN 81 (lift standard).