Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
Автоматизация и управление

      Новости: Автоматизация и управление

      Osiris XUBT: the first Ø 18 cylindrical photo-electric sensor featuring colinear optics

      The first Ø 18 cylindrical photo-electric sensor featuring colinear optics, Osiris XUBT resolves all the problems associated with the delicate detection of transparent materials.

       Its specific optics enable detection from the lens, thus eliminating “blind” zones where previously a risk existed of objects passing unnoticed!

      Perfect detection of facetted or corrugated objects (glass, PET bottles), packaging films, PVC, food containers…. without rebound or magnifying effects.
      Very simple Osiconcept adjustment: A single press on the “teach” button automatically adjusts the XUBT for the majority of applications.
      Plastic or stainless steel (food and beverage processing sector).
      Line of sight along case axis or at 90° to case axis (conveyor systems, packaging).