Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/04/2003

    Romania, a success story in the water treatment sector

    The Romanian subsidiary of "Vivendi Water", "Appa Nova Bucharest", selected Schneider Electric Romania to supply electrical distribution and industrial control equipment, for a total value of 3.2 million euros.
    This is a major breakthrough in the water sector for Schneider Electric's Romanian subsidiary, which has just signed three successive contracts with "Appa Nova Bucharest", valued at 3.2 million euros.

    "Appa Nova Bucharest" was founded by "Vivendi Water", a subsidiary of Vivendi Environnement, specializing in water management. This company is a utility company for the water production, purification and distribution network for the city of Bucharest (population 2 million) for a period of 25 years. This company treats 600,000 cubic meters of water daily and there are plans for Appa Bucharest to invest close to 100 million euros during the next two years to develop and modernize its installations.

    The key factors of success can be summarized in the three following points:
    > The wide range of products and solutions offered by Schneider Electric, meeting control and electrical distribution requirements for the entire water cycle,
    > Experienced and very professional local partners (installers, panel-builders and systems integrators);
    > A relationship of trust with the customer, reinforced by an extensive list of references in the field of water and other industries across the Romanian market.


    The story:
    Recently Schneider Electric Romania won 3 contracts with Apa Nova for projects totalizing 3.2 million euro. The 3 projects are:
    > Rehabilitation of the 6 kV substation at the Rosu treatment plant.
    The project of 400 keuro includes SM6 cubicles with Sepam 1000+ with communication, a PLC network and a Scada system with Monitor Pro.
    > Main LV switchboard at the Rosu treatment plant.
    The project of 200 keuro includes an Okken switchboard locally assembled by one of our licensee with Masterpacts NW with Micrologic 5P integrated in the Scada system, 5 softstarters ATS 48 of 132 kW, PLCs and extension of plant's Scada system.
    >Automation and remote control of pumping and treatment stations of Apa Nova.
    The project of 2.6 million for 2 years includes a large network of Quantum, Premium and Twido PLCs with Modbus and Ethernet communication, 15 Sepam 1000+ with communication, about 15 soft starters ATS 48 and variable speed drives ATV 58, control and protection panels, radio communication, Scada system with Monitor Pro.

    More about Schneider Electric in Roumania: