Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/04/2003

    Hanover Fair 2003 from April 7 to 12

    Schneider Electric will show it's main exhibition in Hall 11 (Booth C64/C72) on over 900 sqm of display net space, presenting the whole range electrical distribution and automation products, as well as application solutions for packaging and conveying. As innovative bricks for building the New Electric World, there is a special focus on :

    Global Detection
    Global detection makes up a complete range of detectors focusing on Osiconcept (offering Simplicity through Innovation) patented by Telemecanique. Osiconcept aims to simplify selection, stockage, installation, setting-up, maintenance and contributes to great improvements in productivity,
    TeSys Model U
    Telemecanique controller-starter combining not only power and control functions, but also control system and communication functions in a single product,
    Phaseo
    A wide Telemecanique offer of single-phase and three-phase regulated switch mode power supplier from 12 to 48 VDC and 7 W to 960 W,
    Evolis
    A new Merlin Gerin MV vacuum circuit breaker from 1 to 17,5 kV.

    According to Hannover Messe AG, the organiser of this event, 6,200 companies from 60 different countries will be at the fair, showing their products on over 210,000 sqm of net display space.
    About 233,000 professionals from 80 countries are expected to visit the Hanover Trade Fair this year.