Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/03/2003

    Public lighting: the Lubio line makes the difference

    The Syndicat Intercommunal d'Electricité (local power utility) in Ain, France, on behalf of the region's central utility in Gex, France sent out a public call for tenders for the renovation of the public lighting control system.

    Schneider Electric has just received an order for 138 units, a sale valued at 225K euros, through its partner Redilec, a panel-builder specializing in public lighting. Delivery will be spread out over an eight-week period and initial commissioning will begin in March 2003.

    The Lubio line offers many advantages:
    > delivers major savings in energy consumption (up to 40%) and in operating costs;
    > compact, modular design for easy integration into existing enclosures and power scalability to match network evolution;
    > The safety of property (by limiting output current) and of people (by maintaining lighting during a power blackout), also has not been forgotten.

    The Lubio line offers the following features:
    > On/off lighting control;
    > Voltage regulation and variation;
    > Measurement of the network's electrical parameters (consumed power, number of hours of operation, etc.).
    It can be used in all types of public lighting networks.


    More about Schneider Electric in France :