Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/11/2002

    Schneider Electric in Morocco

    It is in Fez, one of the country’s four imperial cities, that the Schneider Electric subsidiary in Morocco has just won a very important contract to supply a supermarket from the national chain Marjane with its electrical distribution system. This store, which will cover 10,250 sqm was built in September 2002 and will be open to the public in January 2003.
    Schneider Electric will provide :
    > C60 circuit breakers
    > KS 160 and KN 40 busbar trunking
    > 16 PM500 instrumentation devices
    > 2 draw-out type Compact NS 1600
    > 1 2500A switch
    > All the main outgoing feeders will use NS circuit breakers.

    A new sales office was set up in Agadir on October 1st in order to respond to the needs of customers and fo the type of contract mentionned above . Agadir has become in recent years one of the leading tourist attractions in the country. The subsidiary, which already had its headquarters in Casablanca and an office in Tangiers, has thus expanded its geographic coverage.
    The ambition of Schneider Electric in Morocco is to forge closer links with economic players as well as local and international investors.


    More about Schneider Electric in Morocco: