Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    19/02/2002

    Grands Records: Geronimo bolts like an ocean mustang

    Like a stampeding mustang, the Cap Gemini Ernst & Young and Schneider Electric trimaran has been devouring the miles at a fearsome rate since leaving the start line off Ushant early on Monday morning (02:25:16 French time).
    Led by the present holder of the Trophée Jules Verne, the crew passed Lisbon at around midday as it continued to find its feet at sea.

    Aeolus, the god of the wind, still seems to be smiling on Olivier de Kersauson.
    In favourable weather conditions dominated by strong and sustained northerly winds, the skipper from Finistére has averaged over 21 knots since setting off. "It must be the fastest crossing of the Bay of Biscay I’ve ever done and I’m happy that the crew is really finding its feet on board. For the moment though, we’re not "driving" the boat too hard because I think that it’ll take at least three days for the crew to really feel "at home" with her. We’re doing well, but we must still bear in mind that we’re finding our feet, running in the new mast and haven’t done a lot of sailing over the last couple of months". But despite his quite understandable prudence, Geronimo has still covered 511 miles in her first day at sea at an impressive average speed of 21.29 knots!

    When you realise that Geronimo can carry 1000 m2 of sail, her current performance certainly makes you think, and as Kersauson explained during his daily radio transmission; "In training we achieved some amazing runs in terms of pure speed, but we weren’t timing ourselves then".

    It’s clear then that Yves Pouillaude’s Cap Gemini Ernst & Young watch and Didier Ragot’s Schneider Electric team are, for the time being, holding back from exploiting the fantastic speed potential of their powerful 34-metre trimaran. It’s an attitude that speaks volumes about what we can expect later in this circumnavigation. And as Olivier de Kersauson wisely stresses, "We’ve still got a long way to go" and the adventure has only just begun. The first objective will soon be appearing on their horizon: the equator.

    As they wait to give the horses their heads, the proud warriors of Geronimo are really enjoying the experience of taming North Atlantic waves at the reins of this fantastic ocean mustang.