Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/08/2001

    TeSys recognized

    Mesures, the leading French trade magazine specializing in industrial control, automation and instrumentation, has compensated TeSys in awarding it the Technology Prize in the "automation and actuators" category.
    The Telemecanqiue TeSys range is composed of circuit breakers, contactors and thermal overload relays ensuring motor starter and protection functions, up to power of 75 kW.
    The jury was particularly impressed with the Quickfit solution and the spring connector system enabling motor starters to be implemented without the use of wiring or tools.