Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/03/2001

    Schneider Electric at the 2001 Hannover Fair

    The theme of this year’s Hannover Fair, which runs from April 23 to 28, is “The Power of Industry”. As in 2000, Schneider Electric will have two booths at the event.
    The main location (booth C64 in Hall 11) will present the Company’s expertise in a display covering more than 1,200 square meters. This year’s highlight will be the “Transparent FactoryTM” concept, which embeds Web technologies in industrial automation devices. The solution integrates components into an open architecture based on Ethernet and Internet protocols, allowing users and integrators to leverage new information technologies to reduce system implementation and operating costs. Schneider Electric will also be at the 100 square-meter Safety and Detection booth (D53) in Hall 9 alongside other industry leaders, with all of its latest innovations. Numerous conferences will also be organized.
    To consult the schedule and find out more about Schneider Electric at the Hannover Fair, contact Schneider Electric Germany at www.schneider-electric.de.