Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/09/2000

    Touch’n Click HMI combines safety and innovation

    Touch’n Click is the latest generation of Telemecanique Magelis graphic HMI terminals for automated installations. This particularly innovative solution is based on a technology that combines the comfort of pushbuttons with the flexibility of touchscreens. Touch’n Click’s transparent, mobile keys are attached to the terminal’s touchscreen, thereby eliminating the risk of slippage when the operator makes a selection. The unit’s design also clearly separates the viewing/adjustment area from the control area. Touch’n Click extends the currentMagelis lineup of keyboard and touchscreen terminals and uses Magelis’ XBTL 1000 configuration software.

    For further information, please contact your Schneider Electric representative.