Выберите свою страну/регион в раскрывающемся списке или щелкнув место на карте мира *
Country Selector Alternate Image
 

    Новости

    01/04/2000

    Gazprom compressor station inaugurated in Siberia

    Gazprom invited Schneider Electric CEO Henri Lachmann to attend the inauguration of its new Peregrebnenskaya compressor station in Siberia last month. Schneider Electric supplied 67 Fluair MV draw-out switchboards equipped with Sepam protection units and controlled by an ISIS power management system for the facility. Mr. Lachmann’s trip provided an opportunity for the two groups to strengthen their partnership.

    Gazprom
    Gazprom is the world’s largest natural gas company. It serves nearly 30% of the gas requirements in France, 50% in Germany and 100% in Finland, Austria and the countries surrounding Russia. Gazprom has an installed base of more than 80,000 MV cubicles.