• Default Alternative Text
    Protection of mission critical assets, both from security surveillance and operational monitoring perspectives.

    Infrared Physical Security and Operational Monitoring

Default Alternative Text

Challenges

Remote monitoring: ability to monitor sites 24/7 365 days a year. Not having the ability to monitor critical parameters, both internally and externally on a 24/7 basis has always been a challenge within the industry - until now. Schneider Electric offers robust 24/7/365 day solutions for surveillance and operational monitoring that address safety, regulatory and preventative maintenance needs for all types of facilities.
  • Value Proposition

    Schneider Electric's robust thermal and thermography solutions allow for:
     
    • Integration into various backend systems (VMS, SCADA, HMI, PLC), protection of mission critical assets, both from security surveillance and operational monitoring perspectives.
    • Advanced analytic engine of sending data that can be utilized for trending analysis of key data points, as well as alarms for both parameter and equipment breaches.
    • The ability to send data and/or video to the headend systems allowing for coverage in low bandwidth situations.
  • Differentiation

    Schneider Electric's infrared thermal and thermography solutions are the only ones that allow for:
     
    • Third party integration.
    • Advanced Video Analytics that do not require a license fee.
    • Ability to stream data vs video with embedded data.
Nos conseillers sont disponibles pour répondre à vos questions de 8h00 à 18h00 du lundi au vendredi toute l'année.