Технические FAQs

Задать Вопрос

Where can the embedded Ethernet port of M340 PLC used

The embedded Ethernet port on the M340 processors can be used to connect to the Schneider Electric Magelis range of HMI.

 

For IO scanning NOE module will have to be used as the embedded Ethernet port on the M340 does not support IO scanning.

Вы нашли ответ на свой вопрос?
Как мы можем улучшить информацию?